SNOSB24C October 2008 – November 2025 LM5576-Q1
PRODUCTION DATA
There is a forced off-time of 500ns implemented each cycle to ensure sufficient time for the diode current to be sampled. This forced off-time limits the maximum duty cycle of the buck switch. The maximum duty cycle varies with the operating frequency (see Equation 7).
where
Limiting the maximum duty cycle raisees the input dropout voltage. The input dropout voltage is the lowest input voltage required to maintain regulation of the output voltage. Use Equation 8 to calculate an approximation of the input dropout voltage.

where
Operating at high switching frequency raises the minimum input voltage necessary to maintain regulation.