SNOSDG7A May 2025 – March 2026 TPS7H6101-SEP
PRODUCTION DATA
The external bootstrap capacitor that is required for the driver is connected between BOOT and SW_LS. The bootstrap capacitor voltage serves as the input to the high-side linear regulator BP5H that provides the gate drive voltage for the high-side GaN FET. A general guideline for bootstrap capacitor selection is to specify the capacitance at least 10× greater than the gate capacitance of the high-side GaN FET that is being driven:
Selecting a CBOOT cap value of 1μF satisfies Equation 1.
where:
A more detailed calculation of the minimum bootstrap capacitance needed is show below using Equation 2:
where:
and ∆VBOOT is the maximum allowable drop on BOOT for proper operation:
where:
For applications where the internal bootstrap switch is not used, omit the RSW term from the calculation. Selection of a bootstrap capacitor with low ESR and ESL is recommended. Include in the voltage rating of the bootstrap capacitor sufficient margin above the maximum expected bootstrap voltage.