For SDK introduction and installation,
see Section 3.2.2. If CCS and SDK are installed at the customized address, use the
following steps so that CCS loads SDK successfully.
Select Window → Preferences.
As the MSPM0 SDK is instailled in the C:\ drive, add C:\ as the product
discovery path.
Refresh the Discovered products window. The MSPM0 SDK is recognized
automatically.
Click the Apply and Close
button. The new imported project loads the SDK automatically.