SPMA057E January 2018 – January 2025 TM4C1290NCPDT , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XNCZAD , TMP1826 , TMP1827
Every output pin must be open-drain, and a weak pull up must be attached to the signal so that, the bus is driven low if at least one device drives the bus low. This protocol enables the transfer of data between two devices on the bus while the other devices are in the idle state. The strength of the pull up can be decided by the user based on the following factors: