SPMA057E January   2018  – January 2025 TM4C1290NCPDT , TM4C1290NCZAD , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1297NCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C129CNCPDT , TM4C129CNCZAD , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XNCZAD , TMP1826 , TMP1827

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction to 1-Wire®
    1. 1.1 Bus Requirements
    2. 1.2 Powering
  5. 2Functional Description
    1. 2.1 Signaling on 1-Wire®
    2. 2.2 Address Format of the 1-Wire® Device
    3. 2.3 Typical Communication Flow on the 1-Wire® Bus
  6. 3Functions Available in TivaWare for C Series for 1-Wire® Module
  7. 4Enumeration
    1. 4.1 Legacy Search Algorithm
      1. 4.1.1 Steps of the 3-Bit Search Algorithm
    2. 4.2 Fast Search Algorithm
  8. 5Summary
  9. 6References
  10. 7Revision History

Functions Available in TivaWare for C Series for 1-Wire® Module

Note: ui32Base should contain the base address of the 1-Wire® module.

OneWireBusReset(uint32_t ui32Base); This function issues a reset on the 1-Wire® bus; it does not wait for the completion of the reset.

OneWireBusStatus(uint32_t ui32Base); This function retrieves the bus condition status, which is used to determine if the bus is ready to perform an operation. This status is busy if the host is performing any operation or idle if the host is not performing an operation.

OneWireDataGet(uint32_t u3i2Base, uint32_t *pui32Data);This function waits for the transaction, if any, to complete and retrieves data from the 1-Wire® interface. The data is stored in the address given by pui32Data.

OneWireDataGetNonBlocking(uint32_t ui32Base, uint32_t *pui32Data); This function retrieves data from the 1-Wire® interface. If there is an active transaction, then 0xffffffff is returned. The data is stored in the address given by pui32Data.

OneWireInit(uint32_t ui32Base, uint32_t ui32InitFlags); This function initializes the 1-Wire® module. The ui32InitFlags parameter contains the initialization flags.

OneWireIntClear(uint32_t ui32Base, uint32_t ui32IntFlags); This function clears the required interrupt sources in the 1-Wire® module.

OneWireIntDisable(uint32_t ui32Base, uint32_t ui32IntFlags); This function disables the required interrupt sources in the 1-Wire® module.

OneWireIntEnable(uint32_t ui32Base, uint32_t ui32IntFlags); This function enables the required interrupt sources in the 1-Wire® module.

OneWireIntRegister(uint32_t ui32Base, void(*pfnHandler)(void)); This function registers an interrupt handler for the 1-Wire® module.

OneWireIntUnregister(uint32_t ui32Base); This function unregisters an interrupt handler for the 1-Wire® module.

OneWireIntStatus(uint32_t ui32Base, bool bMasked); This function gets the current interrupt status. If bMasked is true, then the masked interrupt status is obtained. If bMasked is false then the raw interrupt status is obtained.

OneWireTransaction(uint32_t ui32Base, uint32_t ui32OpFlags,uint32_t ui32Data, uint32_t ui32BitCnt); This function is used to perform a 1-Wire® protocol transfer on the bus. ui32BitCnt is used to configure the number of bits to be sent or received. Written data is specified by ui32Data. The ui32OpFlags parameter is used to define which operation (reset, read, write) is to be performed.

Note: More information about the APIs can be found in the (TivaWare™ Peripheral Driver Library User’s Guide).