SPRACA7A October   2017  – September 2022 F28377D-SEP , TMS320F28075 , TMS320F28075-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S

 

  1.   C2000™ Hardware Built-In Self-Test
  2.   Trademarks
  3. 1Introduction
    1. 1.1 HWBIST Overview
      1. 1.1.1 HWBIST Working In-System
    2. 1.2 HWBIST Failure Response
    3. 1.3 Advantages of Using HWBIST In-System
  4. 2Using HWBIST In-System
    1. 2.1 Fundamental HWBIST Operation
      1. 2.1.1 Initializing the HWBIST Controller
      2. 2.1.2 Executing HWBIST
        1. 2.1.2.1 Executing HWBIST Micro-Run
        2. 2.1.2.2 Executing HWBIST Full-Run
      3. 2.1.3 Error Management
    2. 2.2 Managing HWBIST on Dual-Core Device
      1. 2.2.1 Semaphore Management
      2. 2.2.2 Interprocessor Communications
    3. 2.3 System Considerations When Using HWBIST
      1. 2.3.1 Interrupt Latency
      2. 2.3.2 Power Considerations
      3. 2.3.3 HWBIST Memory Requirements
      4. 2.3.4 Injecting Errors
    4. 2.4 Debugging HWBIST In-System
  5. 3References
  6. 4Revision History

HWBIST Failure Response

As mentioned earlier, when the C28x CPU starts the HWBIST controller, the CPU shuts down so that the logic inside can be tested by the HWBIST engine. Figure 1-3 shows the flow of this action in the state diagram.

GUID-19A04843-DABF-41B4-B17C-6001C597498D-low.gifFigure 1-3 HWBIST State Diagram

When the HWBIST detects a failure, it sets the appropriate bit in the HWBIST Status register and exits the HWBIST operation. This error can come in the form of the following:

  • Logic failure was detected
  • HWBIST controller timed out without the micro-run completing

In either case, the HWBIST controller saves the failure information into the HWBIST status register, generates a NMI to the processor, and sets the appropriate bits in the NMI flag register. In a dual processor device, the HWBIST controller generates NMIs to each processor.