SPRACQ1 May 2020 TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28379D , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
There are changes in the control modules between F2837x and F2838x. Most of the control modules on F2838x are of new "Type" compared to F2837x. Also, the number of instance (or channels) have been increased on the F2838x devices. Table 1 shows the module instance differences and module Type differences that should be considered when migrating applications between F2837x and F2838x.