SPRACQ1 May 2020 TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28379D , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S
The F2838x Flash API is enhanced to return an error when an invalid programming mode is provided for program operation. Also, it is enhanced to check the validity of the input address for different functions. Fapi_getLibraryInfo() in F2838x_C28x_FlashAPI.lib returns the Flash API minor version as 60 (F2837xD Flash API returns 54 as the API minor version). Note that the F2838x Flash API library is compiled for EABI format, whereas, the F2837x Flash API library is compiled for legacy COFF. These features are summarized in Table 20
| Feature | F2838x | F2837x |
|---|---|---|
| Library Name | F2838x_C28x_FlashAPI.lib (CPU1/CPU2)
F2838x_CM_FlashAPI.lib (CM) |
F021_API_F2837x_FPU32.lib |
| Library Executable Output | EABI | COFF (with future EABI support) |
| Flash Wait States | Same wait states on both devices | |
| FlashAPI Minor Version | 60 | 54 (F2837xD), 55 (F2837xS) |
For more details, see TMS320F2838x Flash API Reference Guide.