SPRACS4 June 2020 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DK-Q1
JTAGPSWDHx (JTAGPSWDH0 and JTAGPSWDH1) is the upper half of 128-bit JTAG password located in the header section of Zone1 USER OTP of CPU1. Since this is a part of the header, once these values are programmed, it can never be changed again.
JTAGPSWDHx | USER OTP Address |
---|---|
JTAGPSWDH0 | 0x78014 |
JTAGPSWDH1 | 0x78016 |