SPRADD1A August 2023 – September 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM62P-Q1
The following steps set up the custom board devicetrees and configuration files for development. It may be helpful to refer back to the AM62x Devicetree diagram to understand how the devicetrees being created fit into the existing structure.
Create renamed copies of the provided devicetrees using the following commands. If the provided devicetrees are not present in the installed SDK, they can be downloaded in the references section.
$ cp TI_U_BOOT/arch/arm/dts/k3-am625-minimal.dts TI_U_BOOT/arch/arm/dts/k3-am625-<boardname>.dts
$ cp TI_U_BOOT/arch/arm/dts/k3-am625-r5-minimal.dts TI_U_BOOT/arch/arm/dts/k3-am625-r5-<boardname>.dts
$ cp TI_U_BOOT/arch/arm/dts/k3-am625-minimal-u-boot.dtsi TI_U_BOOT/arch/arm/dts/k3-am625-<boardname>-u-boot.dtsiThese naming changes need to be reflected in the #include preprocessor directives in k3-am625-r5-<boardname>.dts.
// in k3-am625-r5-<boardname>.dts
- #include "k3-am625-minimal.dts"
- #include "k3-am625-minimal-u-boot.dtsi"
+ #include "k3-am625-<boardname>.dts"
+ #include "k3-am625-<boardname>.dtsi"The DDR configuration used by U-Boot for DDR initialization is contained in a devicetree that is generated using TI's SysConfig tool. After launching the SysConfig tool and logging in to your myTI account, set the "Software Product" field to "DDR Configuration for AM64x, AM625, AM623, AM62Ax, AM62Px" and the "Device" field to "AM62x". Start the program to load the DDR configuration tool. Here, you can modify DDR settings to match the hardware specification. To prevent signal integrity issues that can lead to boot failure, it is recommended to set the DDR frequency to 667MHz (1334 MTs). This is the slowest speed supported by DDR4 with DLL on. DDR frequency is set in the SysConfig DDR tool's "Memory Frequency (MHz)" field. After completing board bring-up, a new DDR configuration should be generated according to the DDR device specifications. Refer to the SysConfig DDR Configuration README for a complete guide to this tool. The generated file that needs to be included is named k3-am62x-ddr-config.dtsi. Download this file and use the commands below to rename this devicetree and place it in the SDK U-Boot repository.
$ cp k3-am62x-ddr-config.dtsi TI_U_BOOT/arch/arm/dts/k3-am62x-<boardname>-ddr4-<#MTs>.dtsiReplace the following line in k3-am625-r5-<boardname>.dts.
- #include "k3-am62x-sk-ddr4-1600MTs.dtsi"
+ #include "k3-am62x-<boardname>-ddr4-<#MTs>.dtsi"Binman is used to generate U-Boot binaries. Use the following command to duplicate the existing EVM binman devicetree file and rename it for a custom board.
$ cp TI_U_BOOT/arch/arm/dts/k3-am625-sk-binman.dtsi TI_U_BOOT/arch/arm/dts/k3-am625-<boardname>-binman.dtsiIn this newly created file, make the following modification to use the custom devicetree.
- #define SPL_AM625_SK_DTB "spl/dts/k3-am625-sk.dtb"
+ #define SPL_AM625_SK_DTB "spl/dts/k3-am625-<boardname>.dtb"Include this new file in k3-am625-<boardname>-u-boot.dtsi.
- #include "k3-am625-sk-binman.dtsi"
+ #include "k3-am625-<boardname>-binman.dtsi"Newly created devicetrees are added to the Makefile by adding the following lines in TI_U_BOOT/arch/arm/dts/Makefile.
dtb-$(CONFIG_SOC_K3_AM625) += k3-am625-sk.dtb \
k3-am625-r5-sk.dtb \
k3-am62sip-r5-sk.dtb \
k3-am625-beagleplay.dtb \
k3-am625-r5-beagleplay.dtb \
k3-am625-verdin-wifi-dev.dtb \
k3-am625-verdin-r5.dtb \
k3-am625-phyboard-lyra-rdk.dtb \
k3-am625-r5-phycore-som-2gb.dtb \
k3-am62-lp-sk.dtb \
k3-am62-r5-lp-sk.dtb \
+ k3-am625-<boardname>.dtb \
+ k3-am625-r5-<boardname>.dtbCreate or modify two configuration fragments that will be applied on top of the existing AM62x EVM default configuration files to change the devicetree being accessed by U-Boot. These should be created in TI_U_BOOT/configs/. If you followed the steps in Section 3, these files have already been created. Add the lines below to the configuration fragments.
am62x_<boardname>_r5.config
CONFIG_DEFAULT_DEVICE_TREE="k3-am625-r5-<boardname>"am62x_<boardname>_a53.configCONFIG_DEFAULT_DEVICE_TREE="k3-am625-<boardname>"
CONFIG_SPL_OF_LIST="k3-am625-<boardname>"
CONFIG_OF_LIST="k3-am625-<boardname>"The custom board configuration has now been set up within U-Boot.