SPRADD1A August   2023  – September 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP , AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM62P , AM62P-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Installing the SDK
  6. Configuring the SDK for a Custom Board
  7. Starting U-Boot Board Port
    1. 4.1 Introduction to Devicetrees
    2. 4.2 Capabilities of the Minimal Configuration
    3. 4.3 Preparing Custom Board Files
    4. 4.4 Initial Devicetree Modifications
    5. 4.5 Building U-Boot Binaries
    6. 4.6 U-Boot Deployment Instructions
  8. Expanding the Custom Board Devicetree
    1. 5.1 Devicetree Configuration
    2. 5.2 Describing Peripherals in Nodes
    3. 5.3 Revising the Devicetree Configuration
  9. Booting the Linux Kernel
    1. 6.1 Kernel Boot Overview
    2. 6.2 Kernel Deployment Instructions
  10. Tools and Debugging
    1. 7.1 Kernel Debug Traces
    2. 7.2 OpenOCD Debugging
  11. Future Work
  12. Summary
  13. 10References
  14.   Revision History

Starting U-Boot Board Port

Porting U-Boot to a custom board largely involves creating a new devicetree file for the board. This file contains a tree-like structure that describes the hardware to the upper levels of software, in this case U-Boot. For example, this file contains the board specific information to enable a UART port to use as a console output. A basic understanding of the overall devicetree specification will be helpful to complete this file and expedite the porting process.