SPRADH0 August 2024 AM625 , AM6442 , AM69 , TDA4VM
SK-AM62B and TMDS64EVM ran on a real-time Linux operating system, specifically booting using an SD card flashed with the PROCESSOR-SDK-LINUX-RT-AM62x and PROCESSOR-SDK-LINUX-RT-AM64x default wic image, respectively, from Software Development Kit (SDK) version 09.01.00.08.
The TDA4VM and AM69 ran on real-time builds from the respective SDK 09.01.00.06 versions.
CODESYS Control for Linux ARM64 version 4.9.0.0
were manually installed in the Linux root directory by downloading the software
package from the CODESYS website, extracting the ipk package, copying the ipk into
the Linux root directory of the target EtherCAT controller, and extracting the
package with the opkg command.
In addition to the CODESYS Control for Linux ARM64
version ipk package, a CodeMeter application must also be installed to read the
CODESYS license on a CODESYS USB dongle. This must be extracted as a deb package
from the same CODESYS Control for Linux ARM64 downloaded package and manually
installed on the target EtherCAT controller with the opkg
command.
More specific instructions on how to setup the TI embedded processors as EtherCAT controller using the CODESYS stack can be found in Section 7.