The modulation period is the time required to cycle the clock nominal frequency from
an initial value through all the different values along the modulation profile and
back to the initial value. The modulation rate is the inverse of the period.
- The modulation rate is controlled
by the CLKSSCG, the 128-point internal wave table, and the divide value MOD_DIV
as fmod = fCLKSSCG / (128 × MOD_DIV).
- fCLKSSCG =
fREF / REFDIV. With fractional-N mode set for AM62x, AM62Ax,
AM62Px, and AM62Lx:
REFDIV = 1. This means in this
case fCLKSSCG = fREF, where fREF is the PLL
reference clock
(for example, fREF =
25MHz).
- For modulation fidelity, which is
determined by the PLL bandwidth, and to avoid interference with audio
applications, the modulation frequency is typically set above 32kHz and below
fCLKSSCG / 200. For example, the maximum modulation frequency if
a PLL reference clock frequency of 25MHz is used, is 125kHz.