SPRADK2A November 2024 – October 2025 F29H850TU , F29H859TU-Q1
Within the System Security module, the SSUMODE can be selected. As shown in Figure 8-1in SSUMODE 3 secure debug and firmware updates are supported. Thus, to enable debug authorization based on a password entry and match, first select SSUMODE3. After SSUMODE3 has been selected, a section named 'Debug Access (SSU MODE 3 Only)' appears. Within this section, passwords for partial and full debug can be defined for each of the ZONEs. C29 Debug only has one password, hence there is only one entry. These passwords get loaded to SECCFG at the time of boot.
Figure 8-1 SSU Mode 3 additional settingsOnce the device is in SSUMODE3, all debug access is closed. The passwords setup in SysConfig need to be scanned into the device via the SEC-AP interface to open up the proper debug for the different zones. To do this, modify the SEC-AP gel file with the passwords that were used within SysConfig. To access the SEC-AP gel file in CCS, use the following steps:
Upon successful debug open, a connection to the respective C29 cores is possible.