SPRADK2A November 2024 – October 2025 F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1
The Flash SECCFG region is used for storing the User Protection Policy (UPP). This is a special NONMAIN region of the C29 application Flash banks that is dedicated to SSU configuration and boot settings. The settings programmed into SECCFG are loaded at device start-up into SSU memory-mapped registers, and, in most cases, locked until the next device reset. For each primary CPU in the device (that is, odd-numbered C29 CPU, for example: CPU1, CPU3), there are two SECCFG sectors: the base sector, and the reserve sector. These are designed such that one sector can be erased and programmed with new configuration values while the other is active.
.out file to enable the correct update
procedure.To protect the integrity of the SSU user protection policy, the SECCFG sector includes a CRC value that is checked at boot time. This CRC covers access protection settings, LINK and STACK configuration, Flash write and Flash erase protections, Flash update permissions, debug settings, boot settings, and the SSU operating mode. Debug passwords are excluded from this CRC computation.
A comprehensive map of the SECCFG sector is available in the device technical reference manual.