SPRADP7A February 2025 – March 2025 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM67A , TDA4AEN-Q1
This is a simple example of streaming from the camera to a display and visualizing the RGB data. This example demonstrates how the performance metrics listed in Section 3 were benchmarked. The components of the GStreamer pipeline of this example are shown below.
The corresponding GST command can be found in the GitHub repo [6]. To benchmark the performance metrics, this command was run in one terminal console and the perf_stats tool [5] was run in another terminal console simultaneously.
Figure 5-2 Pipeline Throughput of Single
Stream Capture and Visualization
Figure 5-3 CPU, HWA, and DDR Load of
Single Stream Capture and Visualization
Figure 5-4 Pipeline Element Latencies of
Single Stream Capture and Visualization