SPRADU1 September 2026 AM62A3 , AM62A7
This document was translated from a simplified Chinese source. (ZHCAG72)
In automotive and industrial applications, there are many cases where fast boot after power-up is demanded. For example, in an automotive camera monitor system (CMS) or streaming monitor system, the entire process from power-up to display must be completed typically within a few seconds. With the default image used, the boot process of full features often takes more than 20s. The optimization of the boot cycle involves optimizing the boot process, trimming the kernel, and selecting the proper boot media. In this article, the CMS application of the AM62A is used as an example to introduce the fast boot method. In the test described in this article, the duration from power-up to application booting is 2.5s, ideal for the vast majority of applications that demand fast boot.