SPRADU1 September 2026 AM62A3 , AM62A7
Run the following command to generate the .its file.
ATF=$IMAGES_DIR/bl31.bin TEE=$IMAGES_DIR/bl32.bin \
DM=$IMAGES_DIR/ti-dm/am62axx/ipc_echo_testb_mcu1_0_release_strip.xer5f \
/home/ht/ti-processor-sdk-linux-edgeai-am62a-evm-10_01_00_05/board-support/ti-u-boot-2024.04+git/scripts/tispl-linux-falcon.sh \
$IMAGES_DIR/../ti-linux-kernel-6.6.58+git-ti/arch/arm64/boot/Image $IMAGES_DIR/../ti-linux-kernel-6.6.58+git-ti/arch/arm64/boot/dts/ti/k3-am62a7-sk.dtb > tispl-falcon.its
In this command, it is primarily necessary to specify the locations of components in the Falcon binary, such as ATF, TEE, and DM. They must be adapted to the practical circumstances. In the command instance, IMAGES_DIR is the board-support/prebuilt-images folder under the SDK installation directory.
Then run the following command to generate tispl-Falcon.bin
mkimage -E -f tispl-falcon.its tispl-falcon.bin
Running this command generates tispl-Falcon.bin.