SPRADU1 September 2026 AM62A3 , AM62A7
Custom trimming requires modifying the configuration in arch/arm64/configs/defconfig. For example, set CONFIG_PPS to y to compile the code associated with that configuration into the kernel and start it at kernel startup; set the parameter to m to make it a dynamically loaded module, which is loaded when the file system boots after kernel startup is complete; or set the parameter to n to disable it. However, it is important to note that many modules are interdependent, so simply modifying defconfig may not work. The specific effect can be checked after the build by accessing .config under the board-support/ti-linux-xxxx directory under the Linux SDK directory to check the configuration that finally takes effect. For example, although module A is disabled, when module B, which is dependent on module A, is enabled, module A will still be active in .config after the build.
Custom trimming can also be configured using the Linux configuration tool menuconfig, which checks dependencies during configuration to help with efficient configuration.
For example, as the following figure shows, Bluetooth and the associated protocol stack may not be required in the target application. In this case, use menuconfig to open a graphical interface and make a selection with the arrow keys.
Figure 4-1 Menuconfig InterfaceSelecting the Networking support item, you can see a Bluetooth-related option. Select the Bluetooth-related option, and press m to configure the module to be dynamically loaded, press n to disable it, or press y to configure it as a kernel module, which starts with the kernel.
Figure 4-2 Configuring Bluetooth in Menuconfig InterfaceWhen the modifications are complete, select Save.
Figure 4-3 Saving Menuconfig