SPRUJ29A April 2022 – January 2023
For the controlCARD to operate, the controlCARD MCU must be powered. This is done through the USB-C connector on the controlCARD or by inputting 5 V through the HSEC connector using the accompanying baseboard. For example, if using a TMDSHSECDOCK docking station baseboard, 5 VDC can be input into the docking station J1 or J17. Then, S1 needs to be toggled to the appropriate position.
Based on the way the controlCARD is used, additional hardware settings are necessary (see Table 4-1).
| Switch | Debug using CCS IDE and the on-card XDS110 Emulator
(2-pin cJTAG mode, default) | Debug using CCS IDE and an External Emulator using the Baseboard | Standalone (Boot from FLASH or other Boot Mode) |
|---|---|---|---|
| S1:A | Position 1: ON (left, default) to connect the embedded XDS110 emulator to the MCU | Position 1: OFF (right) to disconnect the embedded XDS110 emulator from the MCU | Position 1: OFF (right) to disconnect the embedded XDS110 emulator from the MCU |
| Position 2: ON (left, default) to connect the embedded XDS110 UART COM port to the MCU GPIO28 and GPIO29 pins | Position 2: OFF (right) to disconnect the MCU GPIO28 and GPIO29 pins from the embedded XDS110 UART COM port | Position 2: OFF (right) to disconnect the MCU GPIO28 and GPIO29 pins from the embedded XDS110 UART COM port | |
S2:A | DOWN (default) - Disconnects GPIO35/TDI and GPIO37/TDO from the embedded XDS110 emulator; 2-pin cJTAG mode must be used | DOWN (default) - Disconnects GPIO35/TDI and GPIO37/TDO from the external emulator; 2-pin cJTAG mode must be used | DOWN (default) - Disconnects GPIO35/TDI and GPIO37/TDO from the embedded XDS110 emulator |
| Alternatively this switch be set to UP to connect the GPIO35 and GPIO37 to the embedded XDS110 emulator and enable 4-pin JTAG mode | Alternatively this switch be set to UP to connect the GPIO35 and GPIO37 to the external emulator and enable 4-pin JTAG mode | ||
| S3 | Up (default) - Enables GPIO19/X1 and GPIO18/X2 connection to the on-board XTAL (Y1). | Up (default) - Enables GPIO19/X1 and GPIO18/X2 connection to the on-board XTAL (Y1). | Up (default) - Enables GPIO19/X1 and GPIO18/X2 connection to the on-board XTAL (Y1). |
| Down - Disables GPIO19/X1 and GPIO18/X2 connection to the on-board XTAL (Y1); on-chip INTOSC must be used | Down - Disables GPIO19/X1 and GPIO18/X2 connection to the on-board XTAL (Y1); on-chip INTOSC must be used | Down - Disables GPIO19/X1 and GPIO18/X2 connection to the on-board XTAL (Y1); on-chip INTOSC must be used | |
| Setup S3 as desired | Setup S3 as desired | Setup S3 as desired | |
| S4 | Setup S4 as desired | Setup S4 as desired | Set S4 as desired |
| Putting the C2000 device into Wait Mode can reduce risk of connectivity issues | Putting the C2000 device into Wait Mode can reduce risk of connectivity issues | ||
| J1:A | Connect a USB-C cable between J1:A and your computer | --- | --- |
| In CCS, use this target configuration: TMS320F2800157 device with an XDS110 emulator, 2-pin cJTAG mode (based on S2:A default configuration) | |||
| Baseboard JTAG connector (J2 on Docking Station) | --- | Connect an external emulator | --- |
| In CCS IDE, use this target configuration: TMS320F2800157 device with 2-pin cJTAG mode (based on S2:A default configuration) |
Code Composer Studio™ is an Integrated Development
Environment (IDE) used to debug and develop software for the C2000 series of MCUs.
CCS IDE can be downloaded from the following link:
http://www.ti.com/tool/ccstudio.
Also, GPIO19/X1 and GPIO18/X2 pins are connected on the on-board crystal (Y1) and are not connected to the 120-pin HSEC8 Edge Card Interface.
These and other hardware settings can be modified through switches on the controlCARD. For more details, see Table 4-1.
The following PDF documents are provided, as part of C2000Ware, to describe where each of the F280015x MCU pins appear on the controlCARD connector/docking station:
More information on the controlCARD docking
station can be found in the C2000Ware at the following
location:
<install
directory>\c2000\C2000Ware_<rev>\boards\controlCARDs\TMDSCNCD2800157\Rx_x