SPRUJD4A December 2024 – November 2025 AM62D-Q1
In FIFO interrupt mode (relevant interrupts enabled by the I2C_IRQENABLE_SET register), an interrupt signal informs the processor of the receiver and transmitter status. These interrupts are raised when the RX/TX FIFO thresholds (defined by the I2C_BUF[13-8] RXTRSH bit field value + 1 for the RX FIFO or the I2C_BUF[5-0] TXTRSH bit field value + 1 for the TX FIFO) are reached; the interrupt signals instruct the LH to transfer data to the destination (from the I2C controller in receive mode and/or from any source to the I2C controller FIFO in transmit mode).
Figure 12-50 and Figure 12-51 show receive and transmit operations, respectively, from a FIFO management point of view.
Figure 12-50 I2C Receive FIFO Interrupt Request GenerationIn Figure 12-50 , the RRDY interrupt condition shows that the condition for generating an RRDY interrupt is achieved. The interrupt request is generated when this signal is active, and it can be cleared only by the LH by writing 1 in the corresponding bit. If the condition is still present after clearing the previous interrupt, another interrupt request is generated.
In receive mode, an RRDY interrupt is generated as soon as the FIFO reaches its receive threshold (I2C_BUF[13-8] RXTRSH bit field value + 1). The interrupt can be deasserted only when the LH has handled enough bytes to make the number of bytes in the RX FIFO lower than the programmed threshold. For each interrupt, the LH can be configured to read a number of bytes equal to the value of the RX FIFO threshold.
Figure 12-51 I2C Transmit FIFO Interrupt Request GenerationIn Figure 12-51 , the XRDY interrupt condition shows that the condition for generating an XRDY interrupt is achieved. The interrupt request is generated when TX FIFO is empty or when the TX FIFO threshold is not reached, and the LH can clear the XRDY status bit by setting the I2C_IRQENABLE_CLR[4] XRDY_IE bit to 1 after transmitting the configured number of bytes. If the condition is still present after clearing the previous interrupt, another interrupt request is generated.
In interrupt mode, the module offers two options for the LH application to handle the interrupts:
If the second-interrupt-serving approach is used, an additional mechanism (draining feature) is implemented for cases where the transfer length is not a multiple of the FIFO threshold value (see Section 12.2.2.3.7.3, Draining Feature [I2C Mode Only]).
In target transmit mode (the I2C_CON[10] MST bit is cleared and the I2C_CON[9] TRX bit is set to 1), the draining feature must not be used, because the transfer length is not known at configuration time, and the external controller can end the transfer at any point by not acknowledging 1 data byte. If the draining feature is used in target transmit mode, data can remain in the TX FIFO without being transmitted over the I2C bus. In this case, the TX FIFO must be cleared by setting the I2C_BUF[6] TXFIFO_CLR bit.