SPRZ193T January 2003 – December 2023 SM320F2812 , SM320F2812-EP , SMJ320F2812 , TMS320F2810 , TMS320F2810-Q1 , TMS320F2811 , TMS320F2811-Q1 , TMS320F2812 , TMS320F2812-Q1
eCAN: Abort Acknowledge Bit Not Set
0, A, B, C, D, E, F and G
After setting a transmission request reset (TRR) register bit to abort a message, there are some rare instances where the TRRn and TRSn bits will clear without setting the abort acknowledge (AAn) bit. The transmission itself is correctly aborted, but no interrupt is asserted and there is no indication of a pending operation.
In order for this rare condition to occur, all of the following conditions must happen:
If these conditions occur, then the TRRn and TRSn bits for the mailbox will clear tclr SYSCLKOUT cycles after the TRR bit is set where:
| tclr = ((mailbox_number)*2)+3 SYSCLKOUT cycles |
The TAn and AAn bits will not be set if this condition occurs. Normally, either the TA or AA bit sets after the TRR bit goes to zero.
When this problem occurs, the TRRn and TRSn bits will clear within tclr SYSCLKOUT cycles. To check for this condition, first disable the interrupts. Check the TRRn bit tclr SYSCLKOUT cycles after setting the TRRn bit to make sure it is still set. A set TRRn bit indicates that the problem did not occur.
If the TRRn bit is cleared, it could be because of the normal end of a message and the corresponding TAn or AAn bit is set. Check both the TAn and AAn bits. If either of the bits is set, then the problem did not occur. If they are both zero, then the problem did occur. Handle the condition like the interrupt service routine would except that the AAn bit does not need clearing now.
If the TAn or AAn bit is set, then the normal interrupt routine will happen when the interrupt is re-enabled.