SPRZ455D december 2020 – june 2023 DRA829J , DRA829J-Q1 , DRA829V , TDA4VM , TDA4VM-Q1
ADVANCE INFORMATION
PCIe: Gen2 Capable Endpoint Devices Always Enumerate as Gen1
When a PCIe Gen2 capable End Point (EP) is connected to the SoC configured as a Root Port (RP), the RP fails to enumerate in Gen2 mode and always falls back to Gen1 mode even if autonomous speed change is enabled on both ends of the link.
Once the link reaches L0 state, software can initiate link re-train by setting the PCIE_CORE_LM_I_LINKWIDTH_CONTROL_REG[31] EPLSCRL bit in the PCIe RP. This will force the RP to re-enumerate and achieve Gen2 speed.