SPRZ544C March   2023  – October 2025 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2330
      3.      i2372
      4.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2087
      4.      i2097
      5.      i2134
      6.      i2189
      7.      i2196
      8.      i2199
      9.      i2208
      10.      i2249
      11.      i2278
      12.      i2279
      13.      i2310
      14.      i2311
      15.      i2312
      16.      i2366
      17.      i2371
      18.      i2120
      19.      i2137
      20.      i2190
      21.      i2253
      22.      i2373
      23.      i2383
      24.      i2401
      25.      i2407
      26.      i2409
      27.      i2410
      28.      i2376
      29.      i2399
      30.      i2413
      31.      i2414
      32.      i2419
      33.      i2420
      34.      i2421
      35.      i2422
      36.      i2423
      37.      i2431
      38.      i2435
      39.      i2160
      40.      i2436
      41.      i2482
      42.      i2464
      43.      i2487
      44.      i2493
  4.   Trademarks
  5.   Revision History

i2376

C7x: SE/SA/HWAOPEN receives corrupted template following two back to back VPUT/MVC instructions

Details

On the C7604 CPU, programming information is sent to the Streaming Engines via SEOPEN, the Streaming Address Generators via SAOPEN, and to the MMA via the HWAOPEN instructions. This programming information is sourced from CUCR registers in the CPU that are populated and updated via the MVC and VPUT family of instructions. Data being written into these CUCR registers can be incorrectly forwarded to the SEOPEN, SAOPEN, and HWAOPEN instructions if in a sequence of three CPU cycles a CUCR register is updated on the first two cycles and then used by an SEOPEN, SAOPEN, or HWAOPEN instruction on the third.

For example, this sequence will cause a forwarding error to occur in the execution of the SAOPEN instruction, corrupting SA0's programming:

MVC .C2 VB0, CUCR0
VPUTD .C2 B1, 0, CUCR0
SAOPEN .C2 CUCR1:CUCR0, 0

Workaround

The issue can be avoided by avoiding the sequence of three execute packets where the first two contain MVC/VPUT instructions that write to the same CUCR and the third contains an SE/SA/HWAOPEN instruction that reads from the same. The workaround is included automatically by the compiler when compiling C7504 code.