SPRZ578A December   2024  – July 2025 AM2752-Q1 , AM2754-Q1

 

  1.   1
  2.   Abstract
  3. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  4. 2Silicon Revision Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2284
      2.      i2351
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2120
      4.      i2137
      5.      i2189
      6.      i2196
      7.      i2199
      8.      i2249
      9.      i2253
      10.      i2278
      11.      i2279
      12.      i2310
      13.      i2311
      14.      i2312
      15.      i2377
      16.      i2383
      17.      i2401
      18.      i2427
      19.      i2431
      20.      i2435
      21.      i2436
      22.      i2438
      23.      i2449
      24.      i2455
  5. 3Trademarks
  6. 4Revision History

i2199

C71x: SE returning incorrect data when non-aligned transposed stream crosses AM1 circular buffer boundary

Details:

When AM1 refers to a larger circular buffer size than AM0, SE can reuse the wrong 64B line of data during non-aligned transposed streams. This occurs when one of the rows being transposed crosses the AM1 circular buffer boundary, but not the AM0 boundary.

Workaround(s):

Have the transposed stream either be fully aligned, meaning that the start address and all scaled DIM values be multiples of 64B, or to not configure AM1 to be a larger circular addressing buffers size than AM0.