SPRZ578A December   2024  – July 2025 AM2752-Q1 , AM2754-Q1

 

  1.   1
  2.   Abstract
  3. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  4. 2Silicon Revision Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2284
      2.      i2351
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2120
      4.      i2137
      5.      i2189
      6.      i2196
      7.      i2199
      8.      i2249
      9.      i2253
      10.      i2278
      11.      i2279
      12.      i2310
      13.      i2311
      14.      i2312
      15.      i2377
      16.      i2383
      17.      i2401
      18.      i2427
      19.      i2431
      20.      i2435
      21.      i2436
      22.      i2438
      23.      i2449
      24.      i2455
  5. 3Trademarks
  6. 4Revision History

i2431

BCDMA: RX Channel can lockup in certain scenarios

Details:

BCDMA RX chan Teardown can lockup channel and cannot be used for subsequent transfers if none of the TRs have EOP flag set in configuration specific flags field. Subsequently when channel is re-enabled, transfer does not not complete and terminates with various errors in TR response.

Workaround(s):

a) When receiving data from a PSIL/PDMA peripheral, EOP flag needs to be set in the each TR's configuration specific flag field and PDMA's 1 X-Y FIFO Mode Static TR "Z" paramater can be set to non zero value for channel teardown to function properly and cleanup the internal state memory. Otherwise there can be channel lockups on subsequent runs. The PDMA Z count can also match the TR size, so that PDMA delineates each transfer as an individual packet. This is especially problematic in cases like where TRPD has infinite reload count set to perform cyclic transfer using a single set of TRs in streaming mode, in which case each TR can potentially be the last one.

b) If the usecase doesn't allow for PDMA Z count to be set in advance or packet EOP cannot be set then alternate is to use PKTDMA in single buffer mode instead of BCDMA.