SPVA065 June   2026 TIC12400-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2On-Chip ADC Front-End Architecture Overview
  6. 3Understanding the ILKG Specification in the Datasheet
    1. 3.1 Interpretation of the ±110 µA Specification
    2. 3.2 The Leakage Current Is MUX-Activated and Time-Limited
  7. 4Design Considerations with Weak Voltage Sources
    1. 4.1 Definition of a Weak Voltage Source
    2. 4.2 Mechanism of the Sampling Spike
  8. 5Quantitative Model and Error Estimation
    1. 5.1 Voltage Step During the Sampling Window
    2. 5.2 Steady-State Offset with High-Impedance Sources
  9. 6Design Mitigation Methods
    1. 6.1 Method 1: Strengthen the Voltage Source
    2. 6.2 Method 2: External RC Compensation (Recommended)
    3. 6.3 Method 3: Static Offset Calibration
  10. 7Summary
  11. 8References

Definition of a Weak Voltage Source

In the context of the TIC12400-Q1 ADC input, a weak voltage source is defined as an external source that can accurately establish a DC voltage level but has limited ability to rapidly supply or absorb transient currents. Common examples in automotive BCM and ZCM applications include:

  • Passive resistor divider networks (for example, voltage references derived from a resistor ladder)
  • Slide rheostats used as position sensors
  • High-impedance sensor or transducer outputs that are not actively buffered

These sources can establish DC voltage accurately, but they cannot rapidly absorb or supply transient currents. When the source impedance is low (as in an actively driven output), the transient caused by the MUX-connection current is rapidly absorbed and has a negligible effect on the ADC reading. When the source impedance is high, however, the voltage deviation persists for a duration that can overlap with the ADC conversion window, introducing a systematic offset into the measurement result.