SPVA065 June 2026 TIC12400-Q1
A fundamental understanding of the internal signal chain is necessary to correctly interpret the behavior observed at the INx pins. Figure 2-1 shows the functional block diagram of the TIC12400-Q1, highlighting the ADC front-end path.
Figure 2-1 TIC12400-Q1 Functional Block Diagram
(ADC Front-End Signal Path Highlighted)Each INx input pin is routed to either the ADC or the comparator through an internal multiplexer (MUX). On the ADC signal path, an internal resistive voltage divider scales the external input voltage down to a level compatible with the ADC input range before conversion. Several important architectural characteristics follow from this structure: