SSZTAI4 december 2016
With the solar inverter market growing at a fast rate based on data from International Energy Agency (IEA), it is imperative that designers be able to design their systems faster to meet the market’s needs. But the high voltages of these types of systems require additional care in component selection and system design to develop equipment that operates safely. With system voltages of 1,000 VRMS and 5 V microcontrollers (MCUs) coexisting in solar-inverter systems, isolation between the high- and low-voltage sides is a given. The engineer’s selection of the right digital isolators can help ensure the stability of these systems.
Figure 1 shows a simplified system block diagram of a transformerless grid-tied solar power conversion system. The solar power is harvested by a photovoltaic (PV) panel and processed by post-stage DC/DC and DC/AC converters. The DC/DC converter implements maximum power-point tracking (MPPT) of the solar energy. The DC/AC inverter converts DC power to AC power for interfacing to a utility grid.
Figure 1 Typical System Block Diagram
of a Transformerless Solar Power Conversion SystemA control module processes the feedback signals from the voltage and current sensors, and provides the right sequence and frequency of pulse-width modulated (PWM) control signals to the insulated gate bipolar transistors (IGBT)/ silicon carbide (SiC) MOSFET gate drivers to regulate the voltages and currents of the power converters. The voltage and current regulations are intended to realize MPPT and power-flow control to the grids. The control module interfaces with the rest of the control network through standard communication interfaces such as RS-485, control area network (CAN) or industrial Ethernet.
Additionally, the control module has parts that are accessible to humans; for example, the connectors of the communication interface. Sufficient safety isolation is required between these exposed parts and the high-voltage circuits (circuitry connected to the DC buses and utility grids). Isolated gate drivers, isolated voltage amplifiers and current-sense amplifiers can achieve this isolation. In Figure 1, which shows a human-accessible control module, the input side of the isolated gate drivers and the input side of the isolated amplifiers are referenced to ground, which is safety-isolated from the high-voltage systems. Figure 2 shows how to introduce additional isolation between the control module and communication interface.
Figure 2 Alternative System Block
Diagram of a Transformerless Solar Power Conversion SystemThe International Electrotechnical Commission (IEC) 62109-1 is a safety standard for solar power converters. This standard defines the minimum requirements for the design and manufacture of power-conversion equipment (PCE) for protection against electric shock, energy, fire, mechanical and other hazards. How do you pick the right isolator to address the isolation requirements stipulated by the IEC62109-1 standard? Here’s a simple six-step process that you can follow.