SWRA671 June   2020 CC1312R , CC1312R , CC1352P , CC1352P , CC1352R , CC1352R , CC2652P , CC2652P , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP

 

  1.   Cloning Z-Stack Network Properties Using the SimpleLink Wireless MCU Family
    1.     Trademarks
    2. Introduction
    3. Abbreviations and Acronyms
    4. Tool Versions
      1. 3.1 Command Line Interface (CLI)
      2. 3.2 MAC OS Application
      3. 3.3 Windows Executable
    5. Trust Center and Non-Volatile Memory
    6. Multi-Page NVM
    7. MT Interface
    8. Zigbee Coordinator Setup Procedure
    9. Zigbee Coordinator Cloning Procedure
      1. 8.1 Cloning: Method One
      2. 8.2 Cloning: Method Two
    10. Zigbee Coordinator Cloning Procedure Example
    11. 10 Other Application Considerations
    12. 11 Summary
    13. 12 References
  2.   A TI Zigbee Network Properties Cloning Tool Guide
    1.     A.1 Tool Layout
    2.     A.2 Configuration File
    3.     A.3 Content File
    4.     A.4 Application Selection
    5.     A.5 COM Ports
    6.     A.6 Read Settings
    7.     A.7 Write Settings
    8.     A.8 Output Settings
    9.     A.9 Save/Load Settings
    10.     A.10 Help
  3.   B Establishing a Serial Connection
    1.     B.1 Serial Connections
    2.     B.2 Detecting COM Ports

Cloning Z-Stack Network Properties Using the SimpleLink™ Wireless MCU Family

This application report describes how to clone the coordinator network properties within a ZigBee 3.0 mesh network using the SimpleLink CC13X2 and CC26x2 devices operating from Z-Stack 3.6.0 as included in the SimpleLink CC13X2/CC26X2 v3.4 SDK. The task is accomplished through the use of the TI Zigbee Network Properties Cloning Tool. The tool and its configuration files can be downloaded from the following URL: http://www.ti.com/lit/zip/swra671.