Flash IWRL6432FSPEVM
- Make sure all connections are set
(IWRL6432FSPEVM module, breakout board, USB to UART adapter, micro USB cable to
PC) as discussed in Section 2.3.
- Open the mmWave-L-SDK from Section 1.
- Set the device into Flashing
Mode (SOP1 connected to GND, SOP0 connected to GND). Make sure that the
board is power cycled after the board is switched from Flashing mode to
Functional mode or vice versa.
- Open
MMWAVE_L_SDK_XX_XX_XX_XX\tools\visualizer\visualizer.exe and select
Flash in the left column.
- Select the correct COM port that
the device is connected to (can be found in device manager).
- In the Device Select
section, select XWRL6432. Click NEXT.
- In the Board Switch
Settings section, select SWITCH SETTINGS CONFIRMED.
- In the Image flash
section, select Custom image, then click upload, and upload
MMWAVE_L_SDK_XX_XX_XX_XX\examples\mmw_demo\motion_and_presence_detection\prebuilt_binaries\xwrL64xx\motion_and_presence_detection_demo.release.appimage”.
- Click “Flash”.
Check if Flashing is Successful
- Set the device into Functional
Mode (SOP0=1, SOP1=0). Make sure to power cycle the boards whenever
switching between SOP modes.
- Open PuTTY.
- Select Serial connection
type.
- Input COM port in serial
line.
- Input 115200 speed.
- Click Open.
- When the console opens up, click
Enter, and the output is simliar to Figure 3-3.
- Type version and click
Enter. Check if the module returns the version data in Figure 3-4.
- Connection is set, close
PuTTY.
Running mmWave Visualizer GUI for mmWave Demo
After flashing the IWRL6432FSPEVM, as shown in
Flash IWRL6432FSPEVM, the Plots section in the mmWave visualizer can be used to display range
plot via radar point cloud information.
- Make sure all connections are set (IWRL6432FSP
EVM, breakout board, USB to UART adapter, micro USB cable to PC) as discussed in
Section 2.3.
- Make sure that switch settings are set to
Functional Mode (SOP0=1, SOP1=0). Again, make sure users power cycle
the boards whenever switching between SOP modes.
- Open
MMWAVE_L_SDK_XX_XX_XX_XX\tools\visualizer and select Configuration
Dashboard in the left column.
- In the Device Connection section, enter
the COM Port (can be found in the device manager), Baud rate (115200), and
device (XWRL6432).
- In the Configuration Selection section,
select High Performance Motion Detection for the Select Preset
Configuration section.
- Click Send Config to Device.
- The Plots section needs to then create
plots for the Range Profile, X-Y Plot, Y-Z Plot, and X axis.
- Make sure to power cycle the board between each
configuration that is sent.
- As an example of uploading a local config file,
repeat steps 1-4 above, and select the last option in Configuration
Selection. Then click Upload and upload the
MotionDetect.cfg file that can be found through
MMWAVE_L_SDK_XX_XX_XX_XX\examples\mmw_demo\motion_and_presence_detection\profiles\xwrL64xx-evm.
Click Send Config to Device.
Running mmWave Industrial Visualizer GUI
- Open the GUI by clicking on
Industrial_Visualizer.exe. The GUI is in the folder:
radar_toolbox_XX_XX_XX_XX\tools\visualizers\Applications_Visualizer\Industrial_Visualizer.
- Make sure that the device
selected is the IWRL6432 and the demo selected is IWRL6432 Out of Box
Demo.
- For CLI COM, insert the COM port
number that the device is connected to. Users can check this on the device
manager. If the driver mentioned in Section 2.3 is not installed, then this does not show up.
- Click Connect. If
connected properly, then the GUI displays Connected.
- Open the
Tracking_MidBw.cfg file in the folder:
radar_toolbox_XX_XX_XX_XX\source\ti\examples\People_Tracking\IWRL6432_People_Tracking\chirp_configs\xWRL6432BOOST.
- Click Start and Send
Configuration.
- If this works properly, then the
console and the GUI outputs similar to Figure 3-10.