SWRU628 January   2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 PCB Storage and Handling Recommendations
    2. 2.2 Antenna
    3. 2.3 Setup
  9. 3Software
    1. 3.1 IWRL6432FSP EVM in TIDA-010254 Reference Design
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6References

Antenna

The IWRL6432FSP EVM antenna includes three receive and two transmit FR4 based antennas on the PCB. This has an antenna gain of approximately 5-6 dBi across each antenna. Figure 2-1 shows the antenna configuration.

IWRL6432FSPEVM Receive (Rx) and Transmit (Tx)
                    Antennas of the IWRL6432FSP EVM Figure 2-1 Receive (Rx) and Transmit (Tx) Antennas of the IWRL6432FSP EVM

PCB Material

The dielectric material used for the antenna and transmission lines is FR408HR 0.5 oz dual ply 2x1067 spread glass construction.

IWRL6432FSPEVM IWRL6432FSP EVM PCB Material
                    Stackup Figure 2-2 IWRL6432FSP EVM PCB Material Stackup

Transmitter and Receiver Virtual Array

Transmitter and receiver antenna positions in Figure 2-3 form a virtual array of six transmitter and receiver pairs. This allows object detections with finer azimuthal angular resolution (29°) and coarser elevational angular resolution (58°). Receiver antennas are spaced at distance D (λ/2) in the azithmul plane and D (λ/2) in the elevation plane. Transmitter antenna Tx1 and Tx2 spaced at D (λ/2) in the azimuthal plane and are not spaced out in the elevation plane.

IWRL6432FSPEVM Virtual Antenna Array Figure 2-3 Virtual Antenna Array

Figure 2-3 below shows the antenna radiation pattern with regard to azimuth and Figure 2-4 shows the antenna radiation pattern with regard to elevation. Both figures show the radiation pattern for each TX-RX pair in the complete virtual array. This means that for the -6dB beamwidth, users need to look for a -12dB (Tx(-6dB) + Rx(-6dB)) beamwidth from boresight.

Note: Wavelength (λ) is computed based on a frequency of 62GHz. Antenna placements were designed according to this frequency.
IWRL6432FSPEVM Azimuth Antenna Radiation
                    Patterns Figure 2-4 Azimuth Antenna Radiation Patterns

Measured azimuthal radiation pattern for all Tx-Rx pairs (corner reflector placed at approximately 5 meters with a 4GHz bandwidth chirp starting at 59GHz).

IWRL6432FSPEVM Elevation Antenna Radiation
                    Patterns Figure 2-5 Elevation Antenna Radiation Patterns

Measured elevation radiation pattern for all Tx-Rx pairs (corner reflector placed at approximately 5 meters with a 4GHz bandwidth chirp starting at 59GHz).

CAUTION: In accordance to the EN 62311 RF exposure test, a minimum separation distance of 20 centimeters must be maintained between the user and the EVM during operation.