SWRU637 March 2025
The RF path of the LP-EM-CC2340R53 by default uses the Inverted F antenna printed on its PCB. The SMA connector near the PCB antenna can be used instead, which is useful for tests using an external antenna or for RF-conducted measurements.
To do that, the capacitor CA2 (as shown in Figure 3-1 has to reroute the RF path from the antenna to the SMA: desolder CA2 from its original vertical position (as shown in the picture below) and resolder it horizontally to connect to the pad near the SMA.