SWRU639 February 2025
The two-chip cascade EVM consists of 6-TX channels and 8-RX channels as shown in Figure 2-3 giving a total number of 48 virtual channels in the MIMO virtual array. The arrangement of the channels is shown in Figure 2-4 where the MIMO array gives an aperture limited angle resolution of about 3 deg in the azimuth direction.
The antenna element design is shown in Figure 2-3.
Figure 2-3 TX and RX Channel
Spacings