TIDT244 July 2021
The average of the MB CHG ISNS signal (on TP1) can be used to monitor the output current of the power supply. The following figures show the signal shape for varying output conditions.
Figure 4-15 VIN = 400 V, VOUT = 400
V, IOUT = 2 A.
Figure 4-16 VIN = 400 V, VOUT = 400
V, IOUT = 500 mA.
Figure 4-17 VIN = 400 V, VOUT = 400
V, IOUT = 100 mA.