TIDUEO1B April 2021 – June 2021
Figure 4-1 shows key hardware components. This hardware uses the kit of Bidirectional 400-V/12-V DC/DC Converter Reference Design as the base board and with some modification for peak current mode control.
Figure 4-1 TIDM-02000 hardwareThe key signal connections between the controlCARD and the base board are listed in the Table 4-1
|
SIGNAL NAME |
DESCRIPTOIN |
CONNECTION TO CONTROLCARD |
|---|---|---|
| ePWM-1A | PWM drive for full-bridge switch Q2 | GPIO-00 |
| ePWM-1B | PWM drive for full-bridge switch Q3 | GPIO-01 |
| ePWM-2A | PWM drive for full-bridge switch Q1 | GPIO-02 |
| ePWM-2B | PWM drive for full-bridge switch Q4 | GPIO-03 |
| ePWM-4A | PWM drive for sync rectifier/push-pull switch Q6 | GPIO-07 |
| ePWM-4B | PWM drive for sync-rectifier/push-pull switch Q5 | GPIO-06 |
| VLV-FB | Low voltage bus – voltage feedback | ADC-A0 |
| ILV-FB | Low voltage current feedback (Jumper J2 populated) | ADC-B3/COMP2A |
| ILV-FILT | Heavily filtered low voltage current feedback | ADC-B2 |
| VHV-FB | High voltage bus – voltage feedback | ADC-B1 |
| IHV-FB | Transformer high voltage winding current | ADC-A2/COMP1A |
| IHV-FILT | Heavily filtered transformer high voltage winding current | ADC-A1 |
This board provides a lot of jumper options for experimentation but there are some jumpers that must be populated for proper operation of the board. These jumpers that must be populated are listed below:
C:JPG1, E:JPG1, J2, J5, J6, J7, J8, J10, J11, J12, J13, J15, J16, and J19.
Some hardware modifications are required by the customer before running the reference code in this board.
Figure 4-2 Peak Current Sensing CircuitNotes: Some magnetic components in the original board are replaced for peak current mode control as shown in Table 4-2.
CURRENT | ORIGINAL | |
|---|---|---|
| Main transformer | MPS P6524_A | VITEC AF5551R |
| Secondary side inductor | VITEC 6193R | VITEC AF5666BR |
| Shim inductor | VITEC 6194R | VITEC AF5667BR |
ControlCARD settings:
Certain settings on the device control card are required to communicate over JTAG and use the isolated UART port. The user must also provide a correct ADC reference voltage. The following settings are required for revision A of the TMS320F280049C control card (refer to the info sheet located at \c2000ware\boards\controlCARDs\TMDSCNCD280049C.