TIDUEY1C November 2020 – June 2025 BQ25798
The TPS25751D features two I2C ports: one as a controller port that connects directly to the battery charger. The latter communicates proper configurations for charging mode, charging current, OTG mode, and so forth. The controller port also connects to the I2C EEPROM that contains a patch and configuration bundle which the TPS25751 loads from on boot. The controller port can be used with header J7 to communicate to the BQ25798. The second I2C port, or the target port, can be used to directly program the TPS25751, and program the BQ25798 through the host microcontroller (MCU), or program both, and is available on J3.