TIDUF04A December 2022 – December 2025
The shunt voltage reference (U6) sets the final charge voltage to 7.8 V. The NPN transistor (Q5) and 4.99-Ω resistor (R42) limit the charge current to approximately 120 mA (0.6 V / 4.99 Ω). The NMOS FET (Q4) operates in saturation region to maintain the required charge voltage drop. U6 pulls down the gate of Q4 as soon as Vbackup reaches 7.8 V. This way, Vbackup stays constant at the nominal 7.8 V. There are two charging scenarios:
In summary, the worst-case charging time is 1 minute and 21 seconds, while recharging between energy storage releases is 36.46 seconds.