Figure 4-2 shows the position of these blocks and the connectors on the board. Use the
following steps to set up the test.
- Connect a serial wire debug (SWD) emulator to connector J8 to debug or program
the MSPM01507. Isolate the host PC from TIDA-010250 board.
- Connect a motor cable to the terminals J4, J5, and J6.
- Apply a DC bus power, AC power supply or AC mains power to the inverter by
connecting the power to J1, J2, and J3.
- The maximum output of the
DC power supply is 380VDC.
- The maximum output of the
AC power supply is 265VAC, 50/60Hz.
- AC main power is 220VAC,
50/60Hz.