TIDUFC8 July 2025
This section discusses how to achieve a full-range of ZVS under this DBSRC, related content is now filed for a U.S. patent.
Figure 3-1 and Figure 3-2 provide separate topology schematics and waveforms. In Figure 3-2, θ is the phase angle between Q1 and Q3. According to the analysis in the previous section, to achieve the zero voltage opening of the four switches on the primary and secondary side, t1 must be in the range of 0θ.
Conventional single-phase-shift (SPS) control, as a single-degree-of-freedom control, θ is often used to control power transmission, so this is difficult to make sure that the soft-switching implementation conditions can be met in the full range. Based on this, another degree of freedom, switching frequency, is introduced into this design to provide the realization of a full range of soft switching, which is analyzed in detail in the rest of this topic.
Figure 3-3 shows the bridge voltage VA, VB and resonant current i_res, which is analyzed using the fundamental harmonic analysis (FHA) method, that is, only the fundamental waves of VA and VB are analyzed and normalized. After normalization, the expressions for VA and VB are respectively:
where
where
In Figure 3-2, ires_pu(t1) = 0. From the previously discussed analysis, to make sure all switches achieve zero voltage switching, be sure the t1 value is as expressed in Equation 5.
After considering the accuracy of the FHA and the margin to achieve the ZVS, let t1 = 1/2θ; therefore, Equation 6 is obtained.
Figure 3-3 shows the resonant tank is LC series resonant, so placing the switching frequency at a frequency greater than the resonant frequency fr can make the resonant tank located in the inductive region, so the resonant voltage vres is 90° ahead of the current ires, that is, Equation 7.
Because vres_pu(t) = vA_pu(t) – vB_pu(t), Equation 8 is true.
From Equation 8, solve θ;
By doing this, make sure there is enough current to achieve ZVS for switches in both primary and secondary sides.