TIDUFD9 August 2025
The AFE20408 has up to eight outputs that can be utilized to set the gate bias of eight HPAs and each one can be pulsed between the desired bias point and the pinch-off voltage. The OUT pins can quickly pulse with fast rise and fall times determined by the difference in capacitance between the DAC setting the high-voltage level and the corresponding OUT (for example, DACA0 corresponds to OUTA0, DACA2 corresponds to OUTA2, and so forth). However, the DACA1, DACB1, DACA3, and DACB3 pins have a slower rise time but maintain a fast fall time when pulsing due to higher impedance switches on these outputs. To quickly pulse eight HPAs, an alternative design consideration is to pulse the half bridge leading into the drain of the HPA and then use the eight outputs of the AFE20408 to bias voltage incrementally throughout the operation of the system.