SLUSEW0 December 2023 UCC28750
PRODUCTION DATA
Once finished with the startup state, the device enteres the on state. In this state all of the features of the control law are enabled. The control loop of the system application takes over as the main feedback signal for the control voltage. The FB pin voltage determines the switching operation of the device, and decides if the controller operates in the burst mode, frequency foldback, fixed frequency, or power boost modes, as seen in the Section 7.4.2 section.