JAJSFK1E November 2014 – March 2022 TPS65400
PRODUCTION DATA
The WRITE_PROTECT command disables writes on the PMBus. It has one data byte, described in Table 8-10.
DATA BYTE VALUE | MEANING |
---|---|
1000 0000 | Disable all writes except to the WRITE_PROTECT command |
0100 0000 (default) | Disable all writes except to the WRITE_PROTECT, OPERATION, and PAGE commands |
0010 0000 | Disable all writes except to the WRITE_PROTECT, OPERATION, PAGE, and VREF_COMMAND commands |
0000 0000 | Enable writes to all commands |
If an invalid command is received, a communications fault is set. WRITE_PROTECT does not protect against CLEAR_FAULTS. The user is able to CLEAR_FAULTS anytime regardless of the WRITE_PROTECT state.
This command has no PAGE support.
The WRITE_PROTECT parameter is not stored in the default store in data flash.