SLAA494B May 2011 – September 2023 MSP430AFE221 , MSP430AFE222 , MSP430AFE223 , MSP430AFE231 , MSP430AFE232 , MSP430AFE233 , MSP430AFE251 , MSP430AFE252 , MSP430AFE253
The EVM can be configured to operate with different sources for power specific to the MSP430AFE253 and the MSP430F6638. The various sources of power to the MSP430 devices are JTAG, mains voltage, and external power. Table 6-1 lists the header settings for the power options of the MSP430AFE253 only.
Power Option | JTG_PWR1 | PWR1 |
---|---|---|
JTAG | Jumper on [1-2] | No jumper |
Mains supply | No jumper | Jumper on [1-2] |
External power | No jumper | Jumper on [1-2] |
If JTAG debugging is necessary with external power is ON, the jumper on [2-3] on JTG_PWR1 must be placed in addition to the jumper on PWR1. External power can be provided directly between the DVCC1 and DGND1 headers.
When powered by the mains supply, the PWR1 header can also be treated as a current consumption header by placing an ammeter across it. Also, when powered via JTAG, the current consumption header is no longer PWR1; instead, the ammeter can be connected across [1-2] of header JTAG_PWR1.
Table 6-2 lists the header settings for the power options of the MSP430F6638 only.
Power Option | JTG_PWR2 | PWR2 |
---|---|---|
JTAG | Jumper on [1-2] | No jumper |
Mains supply | No jumper | Jumper on [1-2] |
External power | No jumper | Jumper on [2-3] |
JTAG debugging is necessary with external power is ON. In addition, to jumper on PWR1, jumper on [2-3] on JTG_PWR1 must be placed. External power can be provided directly between DVCC2 and DGND2 headers. In addition for USB power option for the entire board, R15 must be populated and jumper be placed on PWR2 at position [2-3].
When powered by the mains supply PWR2 header can also be treated as a current consumption header by placing an ammeter across. Also, when powered via JTAG, the current consumption header will be no longer PWR2, instead the ammeter can be connected across [1-2] of header JTAG_PWR2.