SLAA494B May 2011 – September 2023 MSP430AFE221 , MSP430AFE222 , MSP430AFE223 , MSP430AFE231 , MSP430AFE232 , MSP430AFE233 , MSP430AFE251 , MSP430AFE252 , MSP430AFE253
The source code is developed in the IAR™ IDE using IAR compiler version 6.x. The project files cannot be opened in earlier versions of IAR. If the project is loaded in a version later than 6.x, a prompt to create a backup is displayed, and you can click YES to proceed. There are two parts to the energy metrology software: