SPRUIY1C November 2020 – April 2024
The AM273x EVM can have a Non-Secure (GP or General Purpose) or a Secure device (HS-FS). To determine if the device is secure, refer to field parameter for security: "y" of the Device name. If the Security Parameter is "H", then the device is a Secure device.
The AM273x device leaves the TI factory in an HS-FS state where customer keys are not programmed and has the following attributes:
The One Time Programmable (OTP) keywriter converts the secure device from HS-FS to HS-SE. The OTP keywriter programs customer keys into the device eFuses to enforce secure boot and establish a root of trust. The secure boot requires an image to be encrypted (optional) and signed using customer keys, which is verified by the SoC. A secure device in the HS-SE state has the following attributes: