- The POK module is the basic block
which is used to monitor a voltage.
- The PRG and PRG_PP module
controls a group of POKs. The PRG samples the output of the POK comparator
throughout a De-Glitch period and flags the voltage as NOT OK if the voltage
violates the limit at every sample.
- One PRG is instantiated within a
POR; the POR module is very nearly an invisible wrapper around the PRG (with
associated POKs).
The POR / PRG(_PP) / POK are arranged
logically in ways defined by Figure 5-2 and a detailed table of how the POKs are integrated is shown in Table 5-9.