SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
A starvation monitor tracks the number of starvation events (a read to an empty queue) that occurred on the queue. The data source is ignored, and the starvation count is always incremented whenever there is a read to the queue and the queue is empty. The count is cleared when the monitor value is read. This can be useful to trigger if any starvation event occurs, or to track how many of these events occur in a timeframe, and can be used for future optimizations or debug.