SPRUJ28C november 2021 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The CSI_RX_IF streams will default to accept all virtual channels and all data types after reset, so the user must program the stream configuration and pixel interface to match the system use case.
The CSI_RX_IF controller can be configured so that the reset values can adopt the users Power_On state. This can reduce the programming steps required by the system.
The CSI_RX_IF controller is designed to operate all the defined streams with all virtual channels and all data types passed to the pixel interface. Also, the connection to the front interface adopts reset values that will allow the connection of the lanes to expect no remapping.
The basic system configuration steps are then programming the number of enabled data lanes and starting the streams.
The system can also decrease the virtual channel and data type processed by the stream by configuring the data config (CSI_RX_IF_VBUS2APB_STREAM0_DATA_CFG - CSI_RX_IF_VBUS2APB_STREAM3_DATA_CFG) registers.
The user must perform a read from the stream config register (CSI_RX_IF_VBUS2APB_STREAM0_CFG - CSI_RX_IF_VBUS2APB_STREAM3_CFG) at power up to identify the number of streams and pixel interface mode. The stream FIFO depth must be determined from the system configuration information defined at build time to ensure that any programmed [31-16] FIFO_FILL level is valid for the available FIFO depth.