SLUSEC2A December 2021 – November 2023 BQ79631-Q1
PRODUCTION DATA
For devices that are daisy-chained to different PCBs through a pair of twisted cables, all three isolation types can be used for daisy-chain isolation. It is also possible to use one type of isolation on one side of the daisy-chain (for example, transformer isolation on COMLP/N to the Battery Management Unit) while using a different type of isolation for the other side of the daisy-chain (for example, capacitor isolation on COMH/N to another BQ796xx Unit).
Option 1: Capacitor Isolation
Components | Value | Description (Capacitor Isolation Between PCBs) |
---|---|---|
RTERM | 1 kΩ | Termination resistor |
RSERIES | 49 Ω | Filter resistor and impedance matching resistor. The connection between devices must be ~120 Ω (~50 Ω on each end of the signal connection of the device plus 10-Ω internal resistance). |
CBYPASS | 220 pF/50 V | Bypass capacitor |
CISO | 2.2 nF | Isolation capacitor Voltage rating depends on application requirement. It is common to select 2x of module voltage rating to provide standoff margin in the event of a fault in the system. |
ESD diode | TVS diode | The ESD protector should provide protection to the communication interface pins during hot-plug events and also for absorption of high-voltage transients during service disconnect or reconnect. Select the ESD diodes to limit the maximum voltage on the COM* bus to below the maximum rating. A voltage rating close to the maximum voltage to provide the highest possible common-mode voltage range is recommended for best EMC performance. The capacitance must be low compared to the coupling capacitance (if using capacitor coupling). |
Figure 9-13 shows the capacitor isolation circuit for devices connecting between PCBs. Similar to the capacitor isolation on the same PCB case, the capacitor must be rated with a high enough voltage to provide standoff margin in the event of a fault in the system that exposes the device to a local hazardous voltage. The voltage is determined by the application requirement but it is common to select 2x of the module voltage.
The capacitance on the daisy-chain bus has a direct effect on performance. All parasitic capacitances from the support components and cabling must be taken into consideration when designing for communication robustness to EMC. Capacitance from the cables, ESD diodes, bypass capacitance, and chokes form a capacitive divider with the isolation capacitors that may affect performance. Additionally, the amount of capacitance on the bus has a direct impact to the operating current during communication (the capacitor charging or discharging).
Option 2: Capacitor Plus Common-Mode Choke Isolation
Components | Value | Description (Capacitor Plus Choke Isolation Between PCBs) |
---|---|---|
RTERM | 1 kΩ | Termination resistor |
RSERIES | 49 Ω | Filter resistor and impedance matching resistor. The connection between devices must be ~120 Ω (~50 Ω on each end of the signal connection of the device plus 10-Ω internal resistance). |
CBYPASS | 220 pF/50 V | Bypass capacitor |
CISO | 2.2 nF | Isolation capacitor Voltage rating depends on application requirement. It is common to select 2x of module voltage rating to provide a standoff margin in the event of a fault in the system. |
Common-mode choke | 100 μH to 500 μH | Common-mode choke An inductance range of 100 μH to 500 μH is a general guidance value, not a specified range as there are many parameters affecting the performance of a common-mode choke. When selecting a recommended part, refer to the SLVAEP4 BQ79616-Q1 Daisy Chain Communications Application Report. The user shall perform the through test in their environment. |
ESD diode (optional) | TVS diode | Optional ESD protection depends on pcb level ESD requirement |
Longer cable lengths, or abnormally noisy applications may require the use of a common-mode choke filter. A capacitor plus choke isolation has better noise immunity than capacitor only. For these applications, use an automotive grade from 100-μH to 500-μH common-mode filter minimum for proper operation. To achieve the best performance in noisy environments, use dual common-mode filters (470 μH). The recommended impedance of the choke is at least 1 kΩ from 1 MHz to 100 MHz and above 300 Ω for higher frequencies.
Option 3: Transformer Isolation
Components | Value | Description (Capacitor Plus Choke Isolation Between PCBs) |
---|---|---|
RTERM | 1 kΩ | Termination resistor |
RSERIES | 49 Ω | Filter resistor and impedance matching resistor. The connection between devices must be ~120 Ω (~50 Ω on each end of the signal connection of the device plus 10-Ω internal resistance) |
CBYPASS | 220 pF/50 V | Bypass capacitor |
Transformer | Inductance: 150 μH to 1400 μH | The inductance range 150 μH to 1400 μH is a general guidance value, not a specified range as there are many parameters affecting the performance of the transformer. When selecting a recommended part, refer to the SLVAEP4 BQ79616-Q1 Daisy-Chain Communications Application Report. The user shall perform the through test in their environment. |
ESD diode (optional) | TVS diode | Optional ESD protection depends on pcb level ESD requirement |
Transformer isolation is supported and can be implemented as above. For example, transformer isolation can be used between the low-voltage and high-voltage boundary for galvanic isolation.